![]()
Global
These are navigation links to move inside this page.
Digital Panel Meters perform digital processing on or conversion and display of voltages, currents, other analog signals, and pulse signals. They can also compare input values to set values, transfer data, and perform other functions.
|
|
Features |
| Principles | Classifications |
| Engineering Data |
|
![]()
Quick links to OMRON IA in your country / territory.
Please contact our European headquarters.
Main Functions
Scaling
Scaling is a function that converts the signal output from various sensors into physical measurement units (pressure, level, flow, etc.) before displaying it.
There are two scaling methods, one of which sets two points: any input value and its corresponding converted value. The other method is teaching by actual inputs.
Position Meter
The present measurement value is displayed as a position in relation to the scaling width on a 20-gradation position meter.
Average Processing
Average processing of input signals with extreme variations eliminates flicker in the display and reduces the effect of noise in the input signal.
There are two types of averages that can be used, the simple average and the moving average.
Forced Zero
It is possible to shift the present value to zero by selecting zero from the front-panel keys. It is useful for setting reference values for measurement.
Timing Chart of a Forced Zero
Timing Hold
Prompted by an external timing signal, it can simultaneously measure the maximum value, minimum value, and the difference between maximum and minimum values.
Maximum/Minimum Hold
Holds the maximum and minimum measurement values.
Display Color Selection
The color of the PV display can be set to either green or red. It is also possible to set the current value to change color according to the status of the comparative output.
Bank Selection
It is possible to switch between eight comparative value banks using the keys on the front-panel or external inputs.
Highly Visible LCD Display with 2-color (Red and Green) LEDs
A Process Indicator Ideal for Discriminating and Displaying Measurements for Voltage/Current Signals
An Ideal Indicator for OK/NG Judgements in Automated and Picking Machines, Measuring Factors such as Pressure, Load, Torque, and Weight Using Load Cell Signal Input.