![]()
Global
These are navigation links to move inside this page.
These Controllers receive sensor signals and control heaters or other devices to maintain a preset temperature. They can also be used for humidity, pressure, and flowrate control. OMRON also provides temperature and humidity sensors.
| Overview | Features |
| Principles |
|
| Engineering Data |
|
![]()
Quick links to OMRON IA in your country / territory.
Please contact our European headquarters.
Temperature Control Configuration Example
The following example describes the basic configuration for temperature control.
Temperature Controller
A Temperature Controller receives electrical signals input from the Temperature Sensor, compares the electrical signal input to the set point, and outputs adjustment signals to the Controller.
Controller
A Controller is used to heat or cool furnaces and tanks using devices such as a solenoid that cuts off electric current to a heater or a fuel valve that shuts off the fuel supply.
Temperature Sensor
The Temperature Sensor consists of an element protected by a pipe. Locate the element, which converts temperatures into electrical signals, in places where temperature control is required.
Temperature Control
The set point is input to operate the Temperature Controller. The time required for stable temperature control varies with the controlled object.Attempting to shorten the response time will usually result in overshooting or hunting the temperature. The response time must not be shortened to reduce overshooting or hunting the temperature.There are applications that require prompt, stable control in the waveform shown in (1) despite overshooting. There are other applications that require the suppression of overshooting in the waveform shown in (3) despite the long time required to stabilize the temperature. In other words, the type of temperature control varies with the application and purpose. The waveform shown in (2) is usually considered to be a proper one for standard applications.
1. The temperature stabilizes after overshooting several times.
2. Proper response
3. The response is slow in reaching the set point.
New 48 x 48-mm Basic Temperature Controller with Enhanced Functions and Performance. Improved Indication Accuracy and Preventive Maintenance Function.
Simple Functions in DIN 48 × 48 mm-size Plug-in Temperature Controllers
Advanced, Compact Digital Controllers