Page top

Primary Contents

Question

How is pressure indicated for E8Y Pressure Sensors?

Answer



The indication method slightly differs between E8Y-A1 and E8Y-A2/A5.

E8Y-A1:
Indicated as 000 Pa to 999 Pa below 1 kPa and, but changes to 1.00-kPa display above 1 kPa.

E8Y-A2/A5:
Indicated as 0.00 kPa to 2.00 kPa or 5.00 kPa whether above or below 1 kPa. Indication is not given in units of 1 Pa.

Recommended Products

E2E

Standard Sensors for Detecting Ferrous Metals under Standard Conditions

E32 Series

OMRON's Fiber Sensors continue to support an increasing range of applications.

FZ2 Series

Real color sensors equipped with 2-million-pixel CCDs, the fastest in the industry. Nine different types of cameras are available.

Other Pressure Sensors FAQ