Page top

Primary Contents

Question

What is the relationship among units of pressure?

Answer



The relationships are given in the following table.

kgf/cm2mmHgmmH2OPa
1 kgf/cm21735.5591.000028 x 1040.0980665M
1 mmHg1.3595 x 10-311.3595 x 100.133322k
1 mmH2O0.99997 x 10-47.356 x 10-210.00980665k
1 Pa(N/m2)1.0197 x 10-57.5006 x 10-30.101971

Examples:

How many kgf/cm2 is 10 Pa?

Pa = 1.0197 x 10-5 (kgf/cm2), so 10 Pa = 10-4(kgf/cm2).

How many Pa is 10 kgf/cm2?

1 kgf/cm2 = 0.0980665 Mpa, so 10 kgf/cm2 = 0.980665 Mpa.

Recommended Products

E2E

Standard Sensors for Detecting Ferrous Metals under Standard Conditions

E32 Series

OMRON's Fiber Sensors continue to support an increasing range of applications.

FZ2 Series

Real color sensors equipped with 2-million-pixel CCDs, the fastest in the industry. Nine different types of cameras are available.

Other Pressure Sensors FAQ