Page top

Primary Contents

Question

What are the dimensions of the slit for slot-type Photomicro Sensors?

Answer



It is the same size as the standard sensing object given in the catalog.

Example: Standard opaque sensing object measuring at least 2 x 0.8 mm for the EE-SX47/67 Series

Dimensions of emitter/receiver slit: 2 x 0.8 mm

Recommended Products

E2E

Standard Sensors for Detecting Ferrous Metals under Standard Conditions

E32 Series

OMRON's Fiber Sensors continue to support an increasing range of applications.

FZ2 Series

Real color sensors equipped with 2-million-pixel CCDs, the fastest in the industry. Nine different types of cameras are available.

Other Photomicro Sensors FAQ