Page top

Primary Contents

Question

Is there an easy way to check whether the control output of the Photomicro Sensors is operating properly?

Answer



The operation can be easily checked with the following procedure using a tester.

Output method and checking procedureDetermination procedure
NPN open-collector output
A resistor is inserted between
and OUT, and the voltage
between OUT and is measured
using a tester.

R: Approx. 4.7 kΩ, 1/2W
The control output is operating property it the
measurement voltage changes to low and high
by the lighting turning ON or OFF. (See note.)
Output statusText measurement voltage
NPN collector load built-in
voltage output
The voltage between OUT and
is measured using a tester.

R: Approx. 4.7 kΩ, 1/2W
Output transistor
ON
L: 1 V max.
(residual output voltage)
PNP open-collector output
A resistor is inserted between
OUT and and the voltage
between and OUT is measured
using a tester.

R: Approx. 4.7 kΩ, 1/2W
Output transistor
OFF
H: Power supply voltage


Note:This is a simple check that determines only whether the control output is malfunctioning.

Recommended Products

E2E

Standard Sensors for Detecting Ferrous Metals under Standard Conditions

E32 Series

OMRON's Fiber Sensors continue to support an increasing range of applications.

FZ2 Series

Real color sensors equipped with 2-million-pixel CCDs, the fastest in the industry. Nine different types of cameras are available.

Other Photomicro Sensors FAQ