![]()
Global
These are navigation links to move inside this page.
![]()
Quick links to OMRON IA in your country / territory.
Please contact our European headquarters.
Question
What malfunction occurs in the Proximity Sensor because of the influence of a surrounding metal?
Answer
The sensing distance is extended, and faulty reset is resulted.
Description
The sensing distance is extended
ON point (ON2) when there is a surrounding metal is further than ON point (ON1) when there is no surrounding metal.
Faulty reset is resulted
There is no OFF point because it lowers more than OFF judgment level even when the sensing object is far and the oscillation level is high when there is a surrounding metal.
Standard Sensors for Detecting Ferrous Metals under Standard Conditions
OMRON's Fiber Sensors continue to support an increasing range of applications.
Real color sensors equipped with 2-million-pixel CCDs, the fastest in the industry. Nine different types of cameras are available.