Page top

Primary Contents

Question

How do I use the screen data transfer port on the NT31/631 Programmable Terminals?

Answer



Use serial port A with the protocol set to "not used."
("Not used" means that the port will not be used for communications with the host. Serial port B cannot be used to transfer screen data.)

With NT31/NT631, it is recommended to use serial port A to transfer screen data, and use serial port B to communicate with the host.

For details, refer to NT31/NT31C Setup Manual or NT631/NT631C Setup Manual.

Recommended Products

NT20, NT31 / 31C-V3, NT631C-V3

Better SYSMAC Compatibility and Easier-to-use Support Software

NS Series

NS-series PTs navigate all areas of machine operation, from daily operation to error recovery.

CXONE-AL[][]C-V4 / -AL[][]D-V4

The CX-One is a comprehensive software package that integrates PLC Programming Software with Support Software for setting up Networks, Programmable Terminals, Servo Systems, Inverters, and Temperature Controllers.

Other Programmable Terminals FAQ