![]()
Global
These are navigation links to move inside this page.
![]()
Quick links to OMRON IA in your country / territory.
Please contact our European headquarters.
Question
What wiring should be used between a Temperature Controller and the G3PX Power Controllers?
Answer
1. Analog Control
Controlling with a 4 to 20-mA-output Temperature Controller
Note: Up to 2 drivable G3PX and a current output Temperature Controller can be used.
This is restricted, however, to Temperature Controllers with an allowable load impedance of 600 Ω.
Changing the Gradient for a Temperature Controller (4 to 20-mA Output)
Note: The gradient can be changed using either the internal or external gradient setting using the external adjuster.
2. ON/OFF Control
Changing Gradient Using a Voltage-output Temperature Controller
Note: The gradient can be changed using either the internal or external gradient setting.