![]()
Global
These are navigation links to move inside this page.
![]()
Quick links to OMRON IA in your country / territory.
Please contact our European headquarters.
Question
How is an electrical current value of the heater calculated?
Answer
The following table shows the different connections possible. The formula under each illustration indicates the electrical current value of the heater elements under normal and abnormal conditions.
Note: Values in this table are correct when a 200 VAC, 1 kW heater is used on a single-phase or three-phase current.
* Wire electric wires of both terminals to the Heater Element Burnout Detector "K2CU Series" correctly.
Digital Time Interval Meter for Measuring Passing Speed, Time, or Cycle between Two Points.