![]()
Global
These are navigation links to move inside this page.
![]()
Quick links to OMRON IA in your country / territory.
Please contact our European headquarters.
Question
What is Simple Average?
Answer
After taking n samples (measurements) this function displays their average value.
The display continues to show the previous value until n samples have been measured.
The displayed value is just the average of n samples, so the previous set of data is unrelated.
This function is useful when you want to lengthen the time between display updates.
Any number of samples can be selected for the simple average.
Note:The output responsive is slower when the readings are averaged.
Applicable models: K3HB-X, K3HB-V, K3HB-S, K3HB-H, K3HB-R, K3GN, K3MA-J, K3MA-F, and K3MA-L Digital Panel Indicators
New 48 x 48-mm Basic Temperature Controller with Enhanced Functions and Performance. Improved Indication Accuracy and Preventive Maintenance Function.
Multiple Operating Modes and Multiple Time Ranges. DIN 48 x 48-mm Multifunctional Timer with Wide AC/DC Power Supply Range for Both High and Low Voltages.
DIN 48 × 48-mm Multifunction Digital Timer/2-stage Digital Timer