![]()
Global
These are navigation links to move inside this page.
![]()
Quick links to OMRON IA in your country / territory.
Please contact our European headquarters.
Question
What is ON/OFF Operation?
Answer
ON/OFF operation is shown in the following illustration.
The output turns ON to provide current to the heater when the present temperature is lower than the set point.
The output turns OFF to shut OFF the heater when the present value is above the set point.
Thus, ON and OFF are repeated near the set point to maintain a constant temperature. This contort method is called ON/OFF operation.
Because the manipulated variable is either 0% or 100% with the set point serving as the boundary, it is also called 2-position operation.
New 48 x 48-mm Basic Temperature Controller with Enhanced Functions and Performance. Improved Indication Accuracy and Preventive Maintenance Function.
Multiple Operating Modes and Multiple Time Ranges. DIN 48 x 48-mm Multifunctional Timer with Wide AC/DC Power Supply Range for Both High and Low Voltages.
DIN 48 × 48-mm Multifunction Digital Timer/2-stage Digital Timer