Page top

Primary Contents

Question

What is the zero cross function?

Answer



The zero cross function causes the Relay to turn ON when the AC load power supply approaches 0 V to suppress noise generated when the load current rises suddenly.

There are two types of noise: noise on power lines and noise emitted into open spaces. The zero cross function is effective against both types of noise.

A very large inrush current flows when lamps and similar equipment are turned ON, but the zero cross function causes the load current to always flow from a point near zero so that inrush current can be suppressed more compared to Solid-state Relays that do not have the zero cross function.

Ideally, the function turns ON near 0 V, but restrictions in the circuit configuration cause it to operate within the range of 0 V ±20 V. This voltage is called zero cross voltage.

Recommended Products

MY

Versatile and Function-filled Miniature Power Relay for Sequence Control and Power Switching Applications

LY

A Miniature Power Relay

G7Z

Multi-pole Power Relay for Contactor Current Range Capable of Carrying and Switching 40 A at 440 VAC

Other Solid-state Relays FAQ