Page top

Primary Contents

Question

What are the differences between WL[][]-2 Limit Switch and WL[][]-2N Limit Switch ?

Answer



The WL[][]-2 has a lever with 90 ° operation to each side, with one-side operation not possible, and a Head that can be mounted in four directions.

The WL[][]-2N has a lever with 90 ° operation to each side, with one-side operation possible, and a Head that can be mounted in two directions.

One-side operation means that three operational directions can be selected electrically, according to the change in the direction of the operating plunger or cam. The three selectable operational directions are "Operate and Operate," "Operate and Not Operate," and "Not Operate and Operate." The models for which one-side operation is not possible can only operate on both sides.

Recommended Products

Z

Best-selling Basic Switch Boasting High Precision and Wide Variety

WL / WLM

Wide Range of Two-circuit Switches; Select One for the Operating Environment/Application

D4A-[]N

The Limit Switch with Better Seal, Shock Resistance, and Strength

Other Limit Switches FAQ