Page top

Primary Contents

Question

The input is not entered into the Programmable Controller when the switch is pressed. Why is this?

Answer



Programmable Controller DC inputs are generally 12 to 24 VDC at a few milliamps. The rated current for general-purpose Basic Switches is 5 to 10 A. Contacts use silver. Sulfide gas and oxidizing gas in the atmosphere form an insulating film on the silver contact surfaces, which results in contact failures. Use Microload Basic Switches that use gold alloy contacts.

Example: Z Basic Switch

Standard model: Z-15GW22-B, Microload model: Z-01HW22-B

Recommended Products

Z

Best-selling Basic Switch Boasting High Precision and Wide Variety

WL / WLM

Wide Range of Two-circuit Switches; Select One for the Operating Environment/Application

D4A-[]N

The Limit Switch with Better Seal, Shock Resistance, and Strength

Other Basic Switches FAQ