Page top

Primary Contents

Question

Is it acceptable to combine SRT1 Slaves and SRT2 Slaves in a CompoBus/S system?

Answer



These Slaves can be combined, but only when the high-speed communications mode is used. They cannot be combined when long-distance mode is being used.

The two kinds of Slaves cannot be combined in long distance mode because the SRT2-series Slaves can be switched between long-distance mode and high-speed mode, but the SRT1-series Slaves support only high-speed mode.

Recommended Products

NT20, NT31 / 31C-V3, NT631C-V3

Better SYSMAC Compatibility and Easier-to-use Support Software

NS Series

NS-series PTs navigate all areas of machine operation, from daily operation to error recovery.

CXONE-AL[][]C-V4 / -AL[][]D-V4

The CX-One is a comprehensive software package that integrates PLC Programming Software with Support Software for setting up Networks, Programmable Terminals, Servo Systems, Inverters, and Temperature Controllers.

Other Field Networks FAQ