Page top

Primary Contents

Question

How do you release lockouts with F3SN/F3SH series Safety Light Curtains?

Answer



The following two methods are used for releasing lockouts.

1.Cycling the power.

2.Applying a reset input.

Releasing Lockouts Using Reset Inputs

Auto Resetting

Apply 24 VDC via a NC reset input switch.

Manual Reset

Apply 24 VDC via a NO reset input switch.

Recommended Products

D4N

Upgraded Safety Limit Switches Based on the Popular D4D, Providing a Full Lineup Conforming to International Standards

F3SJ Ver.2

The updated F3SJ is even easier to use.

OS3101

Operator Presence Detection in Work Areas with Complex Shapes.

Other Safety Sensors FAQ