Page top

Primary Contents

Question

Are there Inverters with RS-422A/485 communications?

Answer



Presently, the following models are capable of RS-422A/485 communications.

3G3MV Series

3G3RV Series

3G3JV Series

Note:In the 3G3JV Series, a 3G3JV-PSI485J RS-422/485 Communications Unit (sold separately) is required to support RS-422A/485 communications.

The communications protocol conforms to MODBUS communications protocol, so no other communications protocols can coexist with the MODBUS. Only Inverter-related products can be connected as Slaves.

Refer to the user's manual for details on the actual communications protocol.

Recommended Products

NT20,NT31/31C-V3,NT631C-V3

Better SYSMAC Compatibility and Easier-to-use Support Software

NS Series

NS-series PTs navigate all areas of machine operation, from daily operation to error recovery.

CXONE-AL[][]C-V3 / -AL[][]D-V3

The CX-One is a comprehensive software package that integrates PLC Programming Software with Support Software for setting up Networks, Programmable Terminals, Servo Systems, Inverters, and Temperature Controllers.

Other Frequency Inverters FAQ