![]()
Global
These are navigation links to move inside this page.
![]()
Quick links to OMRON IA in your country / territory.
Please contact our European headquarters.
Question
Can a single-phase motor be controlled by a 3G3EV Inverter with a single-phase 100-V input?
Answer
No, a single-phase motor cannot be used. Doing so will cause a failure.
The Inverter creates a virtual alternating current with high-speed switching.
If the Inverter is connected to a single-phase capacitor-start induction motor, the capacitor will overheat and burn due to repetitive charging and discharging, so do not connect to this kind of motor.
In addition, if the Inverter is connected to a split-phase-start induction motor or repulsion-start induction motor, the motor's internal centrifugal switch will not operate, and the starting coil may overheat, so do not connect these kinds of motors. Use a three-phase motor.
Better SYSMAC Compatibility and Easier-to-use Support Software
NS-series PTs navigate all areas of machine operation, from daily operation to error recovery.
The CX-One is a comprehensive software package that integrates PLC Programming Software with Support Software for setting up Networks, Programmable Terminals, Servo Systems, Inverters, and Temperature Controllers.