Page top

Primary Contents

Question

I changed the set value of Inverter parameter number n01 to 9 (3-wire sequence), as described in the manual, but the setting changed to 1. Why did it change?

Answer



A setting of 9 causes the Inverter to be initialized in 3-wire sequence mode. When the setting is changed to 9 and the Return Key is pressed, the Inverter is immediately initialized. At this point, the n01 setting is also initialized and reverts to its default setting of 1.

The same phenomenon occurs if the setting is changed to 8.

Think of parameter n01 as a command that initializes the other parameters. Because it is a command, it does not retain its setting like a parameter.

It is normal for n01 to revert to a setting of 1 after initialization.

Recommended Products

NT20,NT31/31C-V3,NT631C-V3

Better SYSMAC Compatibility and Easier-to-use Support Software

NS Series

NS-series PTs navigate all areas of machine operation, from daily operation to error recovery.

CXONE-AL[][]C-V3 / -AL[][]D-V3

The CX-One is a comprehensive software package that integrates PLC Programming Software with Support Software for setting up Networks, Programmable Terminals, Servo Systems, Inverters, and Temperature Controllers.

Other Frequency Inverters FAQ