Page top

Primary Contents

Question

I am moving an Inverter from a location with a 50 Hz power supply frequency to another location with a 60 Hz power supply frequency. Are there any settings that need to be changed?

Answer



One of the features of the Inverter is that it will control operation at the same speed regardless of the power supply frequency.

The Inverter initially converts the input power supply to DC and then converts from the DC power supply back to AC, so differences in the power supply frequency have no effect on operation.

Recommended Products

NT20,NT31/31C-V3,NT631C-V3

Better SYSMAC Compatibility and Easier-to-use Support Software

NS Series

NS-series PTs navigate all areas of machine operation, from daily operation to error recovery.

CXONE-AL[][]C-V3 / -AL[][]D-V3

The CX-One is a comprehensive software package that integrates PLC Programming Software with Support Software for setting up Networks, Programmable Terminals, Servo Systems, Inverters, and Temperature Controllers.

Other Frequency Inverters FAQ