Page top

Primary Contents

Question

When the H7ET-N's Time Counters time range switch is set to 0.0 to 3999d23.9h, what is displayed after 23.9 h?

Answer



100.0 will be displayed after 23.9.
100.0 signifies 1 (day) and 00.0 (hour).
For example, one day and 1.0 hour would be displayed as 101.0.

Supplementary Information
0.1 h indicates 6 minutes.
Therefore, 0.0 will be displayed between 0 to 5 minutes, and 0.1 will be displayed after 6 minutes.

Note:

1.Set the switches before mounting the Unit to a control panel.

2.If the counting speed setting is changed, the present value will not be held. Press the Reset Key on the front panel.

The time unit is given in the datasheet and in the figure above, but on the actual device it will not be displayed. Instead, unit labels (-hours/-d-h/-h-m/-h-m-s) are provided.

Recommended Products

E5CN / E5CN-U (48 x 48 mm)

New 48 x 48-mm Basic Temperature Controller with Enhanced Functions and Performance. Improved Indication Accuracy and Preventive Maintenance Function.

H3CR-A

Multiple Operating Modes and Multiple Time Ranges. DIN 48 x 48-mm Multifunctional Timer with Wide AC/DC Power Supply Range for Both High and Low Voltages.

H5CX

DIN 48 × 48-mm Multifunction Digital Timer/2-stage Digital Timer

Other Counters FAQ