![]()
Global
These are navigation links to move inside this page.
![]()
Quick links to OMRON IA in your country / territory.
Please contact our European headquarters.
Question
Why does the Reset Key on the H7E[]-N not function?
Answer
Is the Key Protect Switch set to ON?
The Key Protect Switch is used to prohibit key operations, thereby preventing incorrect operations.
If the Key Protect Switch is ON, key operations are prohibited and the Counter cannot be reset. To enable key operations, set the Key Protect Switch to OFF.
New 48 x 48-mm Basic Temperature Controller with Enhanced Functions and Performance. Improved Indication Accuracy and Preventive Maintenance Function.
Multiple Operating Modes and Multiple Time Ranges. DIN 48 x 48-mm Multifunctional Timer with Wide AC/DC Power Supply Range for Both High and Low Voltages.
DIN 48 × 48-mm Multifunction Digital Timer/2-stage Digital Timer