![]()
Global
These are navigation links to move inside this page.
![]()
Quick links to OMRON IA in your country / territory.
Please contact our European headquarters.
Question
What is the baud rate of the RS-232C communications port built in to CS1 Programmable Controllers CPU Unit?
Answer
The maximum baud rate when CS or RS control wires are wrapped at ends of the cable is 19,200 bps. When CS or RS control wires and hardware flow control are being used, the maximum achievable baud rate is 38,400 bps in most cases.
When, for example, using a baud rate of 56,000 or 115,200 bps on a laptop computer with the CX-Programmer FA Integrated Tool Package, the hardware chipset, Windows version, installed drivers and application software are all factors that may affect the system, causing stable operations at times and communications errors at other times.
*Windows is a registered trademark of Microsoft Corporation.
Better SYSMAC Compatibility and Easier-to-use Support Software
NS-series PTs navigate all areas of machine operation, from daily operation to error recovery.
The CX-One is a comprehensive software package that integrates PLC Programming Software with Support Software for setting up Networks, Programmable Terminals, Servo Systems, Inverters, and Temperature Controllers.