Page top

Primary Contents

Question

What is the allowable momentary power interruption time for the CQM1-PA203/-PA206/-PA216/-PD026 Power Supply Units?

Answer



If the power is interrupted for less than 10 ms when using a CQM1-PA203/-PA206/-PA216, the Programmable Controller will continue to run normally.
If the power is interrupted for more than 25 ms, the power interruption will be detected, the CPU Unit will stop, and the outputs will turn OFF.
A power interruption that lasts more than 10 ms but less than 25 ms may or may not be detected. Operation in this case cannot be predicted.

If the power is interrupted for longer than 5 ms when using a CQM1-PD026, the power interruption will be detected, the CPU Unit will stop, and the outputs will turn OFF.

Recommended Products

NT20, NT31 / 31C-V3, NT631C-V3

Better SYSMAC Compatibility and Easier-to-use Support Software

NS Series

NS-series PTs navigate all areas of machine operation, from daily operation to error recovery.

CXONE-AL[][]C-V4 / -AL[][]D-V4

The CX-One is a comprehensive software package that integrates PLC Programming Software with Support Software for setting up Networks, Programmable Terminals, Servo Systems, Inverters, and Temperature Controllers.

Other Programmable Controllers FAQ