Page top

Primary Contents

Question

Can Factory Automation System Integrated Tool Package "CX-One CX-Programmer" and Drawing Tool for CX-One NS Series "NS-Designer" be connected with the Programmable Controllers (PLC) by using a USB port built into the personal computer?

Answer



Use the D-sub to USB-Serial Conversion Cable "CS1W-CIF31". This cable can connect the Programmable Logic Controller "SYSMAC" and/or the Programmable Terminal "NT/NS Series" with the support software.

Since Windows softwares including the CX-Programmer and the NS-Designer use the Windows COM port which does not depend on its physical configuration: RS-232C or USB port, either connector can be used. However, since the performance of a commercially-available simple USB-RS232C conversion connector for hobby use may not meet the high-speed communication, utilize a USB conversion cable suitable for FA use

* "Windows" is a registered trademark of Microsoft Corporation.

Recommended Products

NT20, NT31 / 31C-V3, NT631C-V3

Better SYSMAC Compatibility and Easier-to-use Support Software

NS Series

NS-series PTs navigate all areas of machine operation, from daily operation to error recovery.

CXONE-AL[][]C-V4 / -AL[][]D-V4

The CX-One is a comprehensive software package that integrates PLC Programming Software with Support Software for setting up Networks, Programmable Terminals, Servo Systems, Inverters, and Temperature Controllers.

Other Programmable Controllers FAQ