![]()
Global
These are navigation links to move inside this page.
![]()
Quick links to OMRON IA in your country / territory.
Please contact our European headquarters.
Question
What is adjusted in the sensitivity setting of a Photoelectric Sensor?
Answer
The amount of light emitted or the amount of light received are adjusted, and the sensing distance is set.
(The E3X auto tuning type is excluded.)
(1) Through-beam
The amount of light received are adjusted, and the sensing distance is set.
(Refer to below figure)
(2) Reflective, fiber and others
(Emitter and receiver are in the same case)
The amount of light received or the amount of light emitted are adjusted, and the sensing distance is set.
* About the auto tuning amplifier, emitter current and the amount of light received are adjusted depending on a setting distance, and is set to the highest sensitivity.
Standard Sensors for Detecting Ferrous Metals under Standard Conditions
OMRON's Fiber Sensors continue to support an increasing range of applications.
Real color sensors equipped with 2-million-pixel CCDs, the fastest in the industry. Nine different types of cameras are available.