![]()
Global
These are navigation links to move inside this page.
![]()
Quick links to OMRON IA in your country / territory.
Please contact our European headquarters.
Question
Can a Photoelectric Sensor with an Optical Fiber be used in an explosion-proof area?
Answer
Everything except the Amplifier Unit can be used in an explosion-proof area.
Explanation:
A Photoelectric Sensor with an Optical Fiber has no electrical parts, and it can thus be used even in hazardous, explosion-proof areas. However, the lens, the case, and the fiber covering are made of plastic, so they must be free from corrosion or deterioration (fogging) due to contact with solvents.
As long fiber lengths are commonly used in explosion-proof areas, E32-T17L Fiber unit (standard fiber length: 10 m) is recommended.
Standard Sensors for Detecting Ferrous Metals under Standard Conditions
OMRON's Fiber Sensors continue to support an increasing range of applications.
Real color sensors equipped with 2-million-pixel CCDs, the fastest in the industry. Nine different types of cameras are available.