![]()
Global
These are navigation links to move inside this page.
![]()
Quick links to OMRON IA in your country / territory.
Please contact our European headquarters.
Question
What should I be aware of when operating MY2 General-purpose Relays with a transistor?
Answer
Model
| Structure | Plug-in terminals | ![]() | |||
| Classification | No. of poles | With indicator | Without indicator | ||
| Coil surge absorbing diode (coil for DC applications only) ![]() | 2 | MY2N-D2 | MY2-D | ||
| 3 | MY3N-D2 | MY3-D | |||
| 4 | MY4N-D2 | MY4-D | |||
| Double | MY4NZ-D2 | MY4Z-D | |||
Note:
1.Make sure that the polarity is correct.
2.The reset time will be longer but it will still be within 20 ms.
3.Diode characteristics:
Withstand inverse voltage: 1,000 V
Forward current: 1 A