![]()
Global
These are navigation links to move inside this page.
![]()
Quick links to OMRON IA in your country / territory.
Please contact our European headquarters.
Question
What is the best way to estimate the amount of heat produced by the Power Supply?
Answer
The Power Supply's internal loss becomes heat energy (internal loss = heat produced).
Equations:
Internal loss (W)
= Effective input power - Output power
= Output power/Efficiency - Output power
Note:Reducing the load rate is an effective way to reduce the amount of heat produced.
Example Calculating the Heat Produced by a 100-W S82K Switch Mode Power Supply
Power rate: 80%
Output power: 24 V × 4.2 A = 100.8 W
Effective input power: Output power/Efficiency = 100.8 W/80% = 126 W
Internal loss (heat produced): 126 W - 100.8 W = 25.2 W
To convert the internal loss to calories:
By Joule's law, 1 W = 0.24 cal/s,
so 25.2 W = 25.2 × 0.24 cal/s = 6.05 cal/s
Digital Time Interval Meter for Measuring Passing Speed, Time, or Cycle between Two Points.