![]()
Global
These are navigation links to move inside this page.
![]()
Quick links to OMRON IA in your country / territory.
Please contact our European headquarters.
Question
What is the method for turning the output ON and OFF at specific times for the whole year?
Answer
Use the H5S's cyclic operation function.
1. Press the Cycle/Pulse Key.
2. Select all the days of the week (Sunday to Saturday).
3. Set the cycle to start at AM 0:00.
4. Set the cycle to stop at PM 11:59.
5. Set the ON time length.
6. Set the OFF time length.
For the above settings, the output must be OFF for one minute starting at 11:59.
Starting and stopping from different times is also possible.
However, the ON time length and OFF time length combined must be divisible by 24 hours.
New 48 x 48-mm Basic Temperature Controller with Enhanced Functions and Performance. Improved Indication Accuracy and Preventive Maintenance Function.
Multiple Operating Modes and Multiple Time Ranges. DIN 48 x 48-mm Multifunctional Timer with Wide AC/DC Power Supply Range for Both High and Low Voltages.
DIN 48 × 48-mm Multifunction Digital Timer/2-stage Digital Timer