Page top

Primary Contents



Relays

G3NA-205B, G3NA-210B, G3NA-220B, G3NA-410B, G3NA-420B

G3NA-205B_Dim

G3NA-240B, G3NA-440B

G3NA-240B_Dim

G3NA-D210B

Note:The load can be connected to either the positive or negative side.

G3NA-210B_Dim

G3NA-275B-UTU, G3NA-475B-UTU, G3NA-290B-UTU, G3NA-490B-UTU

G3NA-410B_Dim

Options (Order Separately)

One-touch Mounting Plate

The One-touch Mounting Plate is used to mount the GN3A to a DIN Track.

R99-12 FOR G3NA (for the G3NA and G3NE)

R99-12_Dim

Mounting Bracket

R99-11 (for the G3NA-240B, G3NA-440B)

Use Mounting Bracket R99-11 so that the G3NA-240B/-440B can be mounted with the same pitch as that of the G3N-240B.

R99-11_Dim

Heat Sinks

Y92B-N50 Heat Sink (for the G3NA-205B, G3NA-210B, G3NA-D210B, G3NA-410B, G3NE-210T(L))

For surface mounting, a 30% derating of the load current is required (from the Load Current vs. Ambient Temperature graphs.Refer to Datasheet.).
The orientation indicated by the external dimensions is not the correct mounting rientation. When opening mounting holes, refer to the mounting hole dimensions.

Y92B-N50_Dim

Y92B-N100 Heat Sink (for the G3NA-220B, G3NA-420B, G3NE-220T(L))

For surface mounting, a 30% derating of the load current is required (from the Load Current vs. Ambient Temperature graphs.Refer to Datasheet.).
The orientation indicated by the external dimensions is not the correct mounting orientation. When opening mounting holes, refer to the mounting hole dimensions.

Y92B-N100_Dim

Y92B-N150 Heat Sink (for the G3NA-240B, G3NA-440B)

For surface mounting, a 30% derating of the load current is required (from the Load Current vs. Ambient Temperature graphs.Refer to Datasheet.).
The orientation indicated by the external dimensions is not the correct mounting orientation. When opening mounting holes, refer to the mounting hole dimensions.

Y92B-N150_Dim

Y92B-P250NF Heat Sink (for the G3NA-275B-UTU, G3NA-475B-UTU, G3NA-290B-UTU, G3NA-490B-UTU)

The orientation indicated by the external dimensions is not the correct mounting orientation. When opening mounting holes, refer to the mounting hole dimensions.
Observe the precautions given in Mounting Method under Precautions for Correct Use.Refer to Datasheet.

Y92B-N250NF_Dim

Y92B-P250

Y92B-P250_Dim

Y92B-A100 Heat Sink
(for the G3NA-205B,
G3NA-210B,
G3NA-220B,
G3NA-410B,
G3NA-420B,
G3NA-D210B)

Y92B-A150N Heat Sink
(for the G3NA-240B,
G3NA-440B)

Y92B-A100_Dim1
Y92B-A150N_Dim

Y92B-A250 Heat Sink
(for the G3NA-440B)

Y92B-A250_Dim

Mounting Holes
Y92B-A100
Y92B-A150
Y92B-A250

Y92B-A100_Dim2

For surface mounting, a 30% derating of the load current is required (from the Load Current vs. Ambient Temperature graphs.Refer to Datasheet.).
The orientation indicated by the external dimensions is not the correct mounting orientation. When opening mounting holes, refer to the mounting hole dimensions.

Caution: All units are in millimeters unless otherwise indicated.