![]()
Global
These are navigation links to move inside this page.
Smart Power Supply
A New Type of Power Supply That Provides Safety and Maintainability
![]()
Quick links to 'S8AS' page in your country / territory.
Please contact our European headquarters.
Get more support via Products links, such as manuals and CAD files.
Smart Tripping
Branching the Output from a Single Power Supply to Multiple Loads
Variations in the circuit protectors may delaying cutting off some circuits. If the circuit protector does not trip, the protection functions in the power supply will drop the voltage to the other branched circuits. Also, it is difficult to identify the location of the short-circuit, resulting in longer downtimes.
Using the S8AS Smart Power Supply
Any branch output that short-circuits is quickly cut off, with no impact on the other branch outputs. In addition, a branch output that short-circuits is displayed on the monitor, which reduces downtime.
Smart Control Panels
Including the power supply and circuit protection in a single package, greatly reduces design work, wiring work, the number of required wires, and installation space.
This also reduces the maintenance required, as well as number of spare parts that must be kept on hand. Let OMRON make your control panel "Smart."
Smart Functions in a Single Package