![]()
Global
These are navigation links to move inside this page.
Portable Multi-logger
![]()
Quick links to 'ZR-RX20 / RX40' page in your country / territory.
Please contact our European headquarters.
Get more support via Products links, such as manuals and CAD files.
Portable Multi-logger
ZR-RX40
Advanced Fundamentals
All channels isolated
Each circuit is electrically isolated so that the different channels do not affect each other. Consequently, there is no noise interference between the channels giving highly accurate and stable measurements.
Multi-function input
The temperature input supports thermocouples and resistance thermometer. Furthermore, in addition to temperature, an array of measurements including humidity and voltage can be taken at once. It also supports logic or pulse input, input from external triggers, as well as alarm signals output.
Expandable up to 200 channels
(Maximum in its class)
Each detachable terminal block has a standard 20 channels per unit. Up to 10 units can be connected making it possible to extend up to as much as 200 channels. It can also be used in car data logging where multi-measurements of temperature, voltage etc. on many channels is needed. Its seismic resistance corresponds to Class 1-A car parts(JIS standards)which means that it can be used stably even when there are vibrations and jolts during data-gathering.
Outstanding Versatility
Portable size - only 990 grams (Lightest in its class)
Its light weight of 990 gram* makes handheld measurement possible. It is quite portable and can easily be slipped into your brief-case when setting out on a business trip.
*Including 1 terminal unit block. Not including battery or AC adapter.
Easy-to-see 5.7 inch color TFT LCD.
Comes with bright, easy-to-see, high-intensity 5.7 inch TFT large-scale color LCD panel. Its wide field of vision means it can even be seen at an angle.
USB flash drive and internal 12MB flash memory
Inside has a 12MB flash memory. It is also possible to connect it to commercially sold USB flash drive which means that the recording capacity can be selected as required according to application.
*Do not use USB flash drive with security functions.
Potential data recording time(when 10 channels are used)
LAN port enabling remote control from web browser.
Equipped with LAN port for Ethernet connection. By connecting the ZR-RX40 to a PC with a LAN cable, it is possible to set the logger up with your web browser. You can take measurements from your own desktop.
Palm-top Miniature, light-weight
Portable Multi-logger
ZR-RX20
'Easy to operate' and 'easy to handle' means that data can be gathered at ease even from equipment jammed into narrow spaces!
Small but fully-fledged! multifunction input of 10 insulated channels (First in its class)
Even with its small size, the 10 isolated channel input can provide accurate and stable measurements. The ability to input voltage, humidity, pulse and logic, as well as temperature, makes it practical in every field.
Comfortable Usability
(Step1) Connection
No need For Wiring
Detachable terminal blocks - no need for wiring to the main body (ZR-RX40 only)
The ZR-RX40 has removable terminal blocks which means that it can be wired up securely in narrow places just by detaching the blocks. Also, if the terminal blocks are left in the location they have been wired into, there is no need to rewire them back to the main body when you want take repeat measurements.
* Optional parts needed
Connection with just one screwdriver
It uses M3 terminal blocks for analog signal input. The ring terminals and tongue terminals can be easily connected with just one screw driver. There is no need for special tools so it can be used immediately.
(Step2) Installation
No need for AC Adapter
With optional batteries, there is no need for the AC adapter. When fully charged, the ZR-RX20 and ZR-RX40 can run for 6 hours and 9 hours respectively. In the unlikely even that the batteries should cut-out, there is no need to worry as the preceding data is saved with the data back-up function.
(Step3) Configuration- Measurement
No need for operation manuals
Operates just like a mobile phone so you use it just by following your instincts rather than by following the manual. Touching the NAVI button just once brings up a help screen so that you can operate it without the ponderous burden of browsing a manual.
(Step4) Operation- Maintenance
No need for time-consuming work
Easy display and easy editing with PC software
Using the standard PC software provided, graphs can be displayed on a PC, or saved as Excel data. Furthermore, using the optional special PC software, in addition to displaying graphs or saving Excel data, it is possible to monitor multiple measurement data divided into groups, so preparing data for reports is simple.
No need for initial set-up with 3 way PC link (ZR-RX40 only)
3 ways to link to a PC are available through a USB flash drive, a USB connection or a LAN connection. It is also possible to operate with wireless LAN with a commercially available wire LAN to wireless LAN adapter to support your application needs.