Page top

Lead Contents

Smart Sensor (Vision sensor with built-in LCD monitor)

ZFX

ZFX

Essential Innovation for Future Generations

Primary Contents



Application No.220

Measures Both Sides of Embossing Tape to Detect Snaking



Stable detection is achieved with edge measurements of transparent embossing tape moving at high speed.

Application No.222

Detects the Number of Connector Pins



The camera with built-in illumination greatly reduces installation work.

Application No.229

Detects the Positions of Holes Arranged in a Row



Even subtle differences in images are stably detected with a Sensitive Search.

Application No.232

Detects the Number of IC Pins



Edge measurements enable stable counting. More than one area can be counted at the same time.

Application No.233

Orientation of Electronic Components and Detects Incorrect Models



Measuring part of an electronic component's shape or patterns enables determining the orientation of electronic components and detecting incorrect models.

Application No.237

LCD Monitor Inspects for the Presence of Two Dates



High-speed detection of more than one text string is possible with one Amplifier.