![]()
Global
These are navigation links to move inside this page.
Humidity Sensor, Temperature/Humidity Sensor
Detect Humidity within an Accuracy of ±3% in a Compact Body. Controller Set Provides Superior Humidity Control and Temperature/Humidity Control.
![]()
Quick links to 'ES2-HB / ES2-THB' page in your country / territory.
Please contact our European headquarters.
Get more support via Products links, such as manuals and CAD files.
List of Models
| Name | Model |
| Humidity Sensor | ES2-HB |
| Temperature/Humidity Sensor | ES2-THB |
| Humidity Sensor Module (See note.) | ES2-M |
Note: This is a replacement item. One Module is provided with the ES2-HB/-THB. Always attach the Humidity Sensor Module when using the ES2-HB/-THB. Approximately 7 VDC will be output for the humidity output if the Module is not attached or is incompletely attached.