![]()
Global
These are navigation links to move inside this page.
RFID System
New, Next-generation RFID Systems with ISO/IEC 18000-3 (ISO/IEC15693) Compliance
![]()
Quick links to 'V680 series' page in your country / territory.
Please contact our European headquarters.
Get more support via Products links, such as manuals and CAD files.
Versatile Functions for Optimal Use on Production Lines
Conforms to ISO/IEC 18000-3 (ISO/IEC 15693)
Can be used in many countries around the world.
The V680 Series can be used in many parts of the world because it meets the requirements of radio wave regulations in Japan, Europe, the U.S.A., Canada, Mexico, Singapore, Malaysia, the Philippines, China, Hong Kong, Taiwan, and Korea. Contact your OMRON sales representative for details on use in other countries.
Note:The requirements of radio wave regulations have been met in the countries listed above for combinations of a V680-HA63A or V680-HA63B Amplifier and a V680-HS52, V680-HS63, or V680-HS65 Antenna (application pending in Mexico). The V680-CH and V680-H01 Antennas and combinations of a V680-HA63A or V680-HA63B Amplifier and a V680-HS51 Antenna meet the requirements of radio wave regulations in Japan, Europe, the U.S.A., and Canada. Application is in progress in other countries.
Enables High-speed Data Transmission
High-speed transmission of 27 kbps achieved.
The V680 Series offers data transmission speeds as high as 27 kbps at an operating frequency of 13.56 MHz, and dramatically shortens turn around time (TAT) with a Self-execution Mode that eliminates the need for host access.
A Wide Range of ID Tags Available for Various Production Lines
These ultra-compact Tags also feature high environmental durability, long service lives, and maintenance-free operation.
ID Tags can be either embedded in metal or mounted on non-metallic objects without requiring any extra attachments.
A long service life enables 10 billion accesses.
A new battery-less model with a large, 32-Kbyte capacity has been added to the line-up.
In addition to managing the growing amount of production and quality data on today's factory floors, this new Tag makes it easy to build a system with traceability.
The V680 Series features the same level of environmental durability as the previous V600 Series.
No Changes Needed when Switching from an Existing System
The V680 Series also supports V600-series commands, so there is no need to change command systems.
Easier Startup and Maintenance.
Simpler Operation.
Lets You Visualize Data Transmission
Contributes to higher efficiency for on-site startup and maintenance.
Seven maintenance modes make it easy to diagnose the optimal usage conditions for the V680 RFID System.
Startup is also easier because the system can be checked without having to use a personal computer or other host device.
Strong Support for Creating ID Tag Memory Maps
Using the ID Map Manager dramatically shortens the time required to allocate ID Tag memory and complete system designs.
Work efficiency is greatly increased because the ID Map Manager includes an ID Tag read/write test function and communications checking function in addition to memory map definition and editing functions.
Memory map data created by the ID Map Manager can also be easily shared between the production line design department and the vendors that are building the line.
Visualize Data Transmission without the Need for a Host Device.
Perform Simple Diagnosis of Communications Conditions.
Distance Level Measurement Mode
Confirms correct mounting positions for the Read/Write Antenna and ID Tag.
The distance between the Read/Write Antenna and ID Tag mounting locations relative to the communications range is displayed using six levels.
Noise Level Measurement Mode
Confirms spatial noise, noise sources, and noise countermeasure effects.
Measures the ambient noise level and displays it in levels ranging from 00 to 99.
Speed Level Measurement Mode (Read/Write)
Confirms the speed of moving ID Tags and the number of usable bytes.
Data is transmitted repeatedly to moving ID Tags, and the number of successful communications and speed level are displayed in levels ranging from 01 to 99.
(No data is actually written to the ID Tags during the write part of the Speed Level Measurement Mode.)
Seven maintenance modes make it easy to diagnose the communications conditions from the front panel of the Controller or Amplifier Unit. The data can also be output from the USB port of the Controller to a personal computer or other monitoring device.
(Maintenance Mode cannot be used with the V680-H01 or V680-CH.)
Communications Success Rate Measurement Mode
Confirms the communications success rate between the Read/Write Antenna and ID Tags.
A total of 100 communications are executed without retries, and the rate of communications success is displayed in levels ranging from 01 to 99.
Host Device Communications Monitor Mode (Protocol Analyzer Function)
This mode can be used as a protocol analyzer function for host device communications lines.
The communications commands sent from the host device and the execution result responses can be output from the USB port of the Controller.
Tag Communications Test Mode
Confirms communications ability between the Read/Write Antenna and ID Tags.
The end codes are displayed to show the results of communications between the Read/Write Antenna and ID Tags. When the Controller is mounted inside a control panel, or in some other location, this data can be output from the Controller's USB port and easily checked on a monitor.
(The Tag Communications Test Mode uses only read operations.)
Host Device Communications Confirmation Mode
Confirms whether the signals sent from the Controller are being correctly transferred to an external device.
The communications commands and responses between the Controller and a host device are output from the Controller's USB port for easy identification of problems, such as incorrect communications parameters or wiring.