Page top

Lead Contents

Smart Sensors 2D Profile Measuring Sensors

ZG

ZG

Ultra Wide Laser Beam & Super High-speed Measurement

Primary Contents



A wide laser beam captur esentire shapes with ease.

A new Smart Sensor debuts with a light-section method that visualizes cross-sectional shapes.

ZG_Features1

Three basic steps

An advanced interface maximizes the sensing performance with extremely simple operation.

1st Display the profile.

ZG_Features2

The profile is displayed as soon as the power is turned ON.*
The Sensor Head position can be adjusted while viewing the profile on the screen.

*In FUN mode.

2nd Select the measurement item.

ZG_Features3

Select the icon for the item to be measured, such as height, step, or cross-sectional area.

3rd Designate the measurement range.

ZG_Features4

Simply enclose the range to be measured with the box. The ZG automatically optimizes the sensing conditions.

*Screen images are simulated.

High-speed Inspection

High-speed, continuous sampling meets the needs of processes where speed is required.

Inspecting fluid application for formed-in-place gaskets (FIPG) (ZG-WDS22/70)

ZG_Features5

Measure continuous motion on a robot arm

Continuously output profiles

High-speed processing technology

Equipped with the PI-Express image processing core engine. (Newly developed)

Principle

ZG_Features6

All processing is done digitally, from sensing input to output. The generation of shape profile data and measurement functions that were conventionally handled by a microprocessor are built into a single chip.
Use of the newly developed PI Express (see note) LSI speeds up processing and saves space.

Note:Profile- Image-Express

Effect

ZG_Features7

The response time required from receiving an external input (trigger) to outputting complete profile data via USB is 100 ms (see note) maximum.

Note:Varies depending on the measurement mode.

Highprecision Shape Measurement

The shape of the measurement object is completely reproduced with high precision.

Inspecting vehicle body gaps (ZG-WDS22/70)

ZG_Features8

High-precision measurement of the width of grooves during vehicle assembly

Multi-sensitivity Function (Patent Pending)

When a laser is directed at a complicated shape, the light often does not effectively reflect from parts on which the beam strikes at an angle.
This causes a part of the profile to be lost and makes it impossible to reproduce the shape.
The multi-sensitivity function of the ZG-series 2D Shape Sensors determines the optimal sensitivity for each line to reproduce the shape profile.

Principle

While switching sensitivity levels for workpieces with reflectivity that varies from part to part, the Sensor inputs multiple images and combines them into a single image with the optimal sensitivity for each part. This produces an image of the entire workpiece.

ZG_Features9

Example: A mountain-shaped workpiece in which the reflectivity varies from that of the reference plane.

Effect

ZG_Features10

Simple Shape Measurement

Teaching enables simple shape distinguishing and positioning.

Distinguishing the shape of a pin boss (ZG-WDS22)

ZG_Features11

Convex or concave pin bosses can be easily distinguished.

Checking the shape of vehicle structural parts (ZG-WDS22)

ZG_Features12

The wide beam allows vehicle structural parts to be measured in a single operation.

Reflective-type Sensor

Installs easily just about anywhere.

The wide beam enables stable, reflective measurement when mounting limitations do not allow a through-beam configuration to be used or when measuring the ends of warped panels, which is difficult for through-beam systems.

Highprecision Displacement Sensor

Virtually any object can be measured.

The advantages of the wide beam are not limited to shape measurement. The line beam averages slightly irregular reflections from a bumpy surface to provide a level of precision that was not possible with conventional displacement sensors.

Measuring the thickness of metal panels while they are being conveyed

ZG_Features13

Measuring the end of warped panels

ZG_Features14

OMRON ZS-series Displacement Sensor

ZG_Features15

ZG Series

ZG_Features16

Note:Shows the result of using the entire line, with the Sensor being used as a wide displacement gauge.

Flexible Mode Selection - From High Speed to High Precision

Flexible Measurement Technology (Patent Pending)

Principle

Light-section method

Effect

Functions to alter the measuring precision in the displacement direction and change the sampling period are provided for the first time on a displacement sensor using the light-section method.
Also, installation is easy because the measurement center distance remains fixed even when the measurement made is changed.

ZG_Features17

High-speed Mode

A fast 5 ms satisfies the needs of processes that require speed.

ZG_Features18

Measuring chip height above a lead frame (ZG-WDS3)

High-precision Mode

Completely reproduces the shape of the measurement object to measure with high precision.

ZG_Features19

Measuring the shape of air-bag grooves (ZG-WDS8)

Trigger Synch Measurement

Featuring an operation mode that calculates the measurement value in synch with the command input!

An external command (parallel input with USB 2.0 or RS-232C) can be used in either the fixed or multi sensitivity mode to obtain data at the desired timing.

Conventional model

It was not possible to designate the timing for external measurement requests.

ZG_Features20

Z G

Measurement values can be obtained for specific measurement cycles in response to external measurement requests.

ZG_Features21

The Inspection Status Is Immediately Visible

A Compact, All-in-one Controller with LCD Monitor

Sensor-captured status is completely reproduced as a profile.

ZG_Features22

The multifunctional Controller has been condensed to the industry's smallest size so it can be installed wherever it is required, to give precisely the number of inspections that are necessary.

Enlarged Display of Profiles on a Personal Computer

Smart Monitor ZG Setup Support Software

Using the included Smart Monitor ZG Setup Support Software (see note), intricate profiles that cannot be sufficiently checked on the Controller's LCD monitor can be displayed and checked on the large screen of a personal computer.

ZG_Features23

Recommended Operating Environment
Smart Monitor ZG Setup Support Software
OS: Windows 2000/XP
CPU: Pentium III 850 MHz or faster (2 GHz or faster recommended)
Memory: 128 MB or more (256 MB or more recommended)
Available hard disk space: 50 MB or more
Display: 1024 x 768 dots, True Color (32-bit) or higher

Note:Standard equipment with the ZG-WDC[][]A Controller