Page top

Primary Contents



One-piece completely stainless-steel housing with a face thickness of 0.8 mm

The face thickness is approximately 4 times that of previous models (E2ES) to enable sensing in even more severe conditions than ever.

E2FM_Feature1

Brush Test

Continuous Impact Test

E2FM_Feature2
E2FM_Feature3

Chemical and Detergent Proof

The one-piece completely stainless-steel housing of the sensing section withstands the following chemicals better.

Sodium chloride

Gasoline

Dilute sodium hydroxide

Dilute hydrochloric acid

Mineral oil

Barium hydroxide

Any many others

Note:Cannot be used for explosion-proof applications.

Built-in Chip Immunity

Chip immunity performance has been provided to greatly reduce false signals caused by spatter accumulation and other causes, almost eliminating the needs for cleaning, e.g., with metal brushes.

E2FM_Feature4

Flush Mounting

E2FM_Feature5

Main Performance Comparison to Previous OMRON Products

E2FM_Features6

The chemical resistance has been certified by Ecolab Europe

E2FM_Feature7