![]()
Global
These are navigation links to move inside this page.
Smart Sensors 2D CMOS Laser Type
Very High-performance Sensors that Support Core Quality from Very Long-range to Extremely Precise Measurements
![]()
Quick links to 'ZS-HL' page in your country / territory.
Please contact our European headquarters.
Get more support via Products links, such as manuals and CAD files.
Very High-performance Sensors that Support Core Quality from Very Long-range to Extremely Precise Measurements
Range of models with measuring center distance of 20 to 1,500 mm.
Achieves maximum resolution of 0.25 μm.
Maximum response speed of 110 μs.
Parallel output supported.
Extreme Stability
Ideal Size and Stability
Head Size
Complete sensing stability with optimum Sensor Head size for best performance and holding mechanism secured at 3 points. (See note.)
Note:ZS-HLDS2T not applicable.
Superior Moving Resolution
Increased Lens Resolution
Moving resolution (error based on workpiece surface position) has been reduced dramatically by optimizing the optical system with increased sensitivity and resolution of the light receiving lenses.
Reduced Error for Different Materials
2D CMOS
With a CCD, the charge overflows to the next pixel when excessive light is received. This phenomenon does not occur with CMOS, so there are no effects from light fluctuations from different materials or excessive light reception.
ZS-HLDS5T/HLDS10
Detect Essentially Any Object
Reduced Variation in Linearity between Different Objects, and Linearity Determines Measurement Accuracy.
Makes it easier to introduce a variety of detection objects.
Measuring Car Body Widths
(ZS-HLDS10)
Manage trends by measuring widths of each car model.
Linearity Characteristic
ZS-HLDS60/HLDS150
A Long Range That Handles Essentially Any Installation Site
First 1,500 mm long range sensing in the industry enables measurement of previously impossible points.
Simple Long-distance Step Measurement
Note:This function may not be applicable in bright surrounds.
ZS-HLDS2VT
Ideal for Measuring the Height and Thickness of Transparent Objects
Tilted and moving workpieces can also be stably measured.
A special aspherical lens was developed for the ZS-HLDS2VT, and the design of the optical structure was optimized for regular-reflective workpieces. This has greatly increased the allowable degree of tilt and improved stability for measuring transparent and regularreflective workpieces.
Angle Characteristics
ZS-HLDS2T/ZS-LD10GT/LD15GT
The Only Way to Very High-precision Measurements
Superior Features for Semiconductor Wafer, Glass, and Other Measurements Requiring Precision
Simultaneous Measuring of Touch Panel Film Thickness and Gap
An unbelievable stationary measurement precision of 0.25 μm, the highest in this product class.
Ideal for Measuring Nozzle Gaps!
Reduced pattern influence for moving measurement, the best in the moving resolution industry.
Possible to match nozzle drip point and measurement point then measure.
Sensor Head with separate light emission and reception in one unit to create nozzle space.
Height Control of Sealant Dispensers
Inspection of Disk Play on HDD Motor Rotating Plate