![]()
Global
These are navigation links to move inside this page.
FA Integrated Tool Package
The CX-One is a comprehensive software package that integrates PLC Programming Software with Support Software for setting up Networks, Programmable Terminals, Servo Systems, Inverters, and Temperature Controllers.
![]()
Quick links to 'CXONE-AL[][]C-V3 / -AL[][]D-V3' page in your country / territory.
Please contact our European headquarters.
Get more support via Products links, such as manuals and CAD files.
System Requirements
| Item | Requirement | |
| Operating system (OS) (See note 1.) Japanese or English system | Microsoft Windows 2000 (Service Pack 3 or higher) or XP | Microsoft Windows Vista (See note 4.) |
| Computer | IBM PC/AT or compatible with a Pentium II 333 MHz or faster processor (Pentium III 1 GHz or faster recommended.) | IBM PC/AT or compatible with a processor recommended by Microsoft. (1 GHz or faster recommended) |
| Memory | 256 MB minimum (See note 2.) | 512 MB min. required.1 GB min. recommended. |
| Hard disk | Approx. 2.8 GB or more available space is required to install the complete CX-One package | |
| Display | SVGA (800 × 600) or better high-resolution display with 256 colors min. | |
| Disk drive | CD-ROM drive or DVD-ROM drive | |
| Communications ports | RS-232C port, USB port, or Ethernet port (see note 3.) | |
| Other | Internet access is required for online user registration, including a modem or other hardware connection method. | |
Note:
1.CX-One Operating System Precaution System requirements and hard disk space may vary with the system environment.
2.The amount of memory required varies with the Support Software used in CX-One for the following Support Software. Refer to user documentation for individual Support Software for details.
CX-Programmer, CX-Designer, CX-Thermo, CX-Simulator, CX-Protocol, CX-Motion, CX-Drive, CX-Process Tool, and Faceplate Auto-Builder for NS.
3.An RS-232C port is required to connect the Support Software in CX-One to a PLC. If the computer provides only a USB port, use a CS1W-CIF31 USB-to-RS-232C Conversion Cable. For connecting to the CP Series,however, an over-the-counter USB cable (type A-B) can be used.
For the CX-Drive, the CS1W-CIF31 USB-to-RS-232C Conversion Cable cannot be used to connect a USB port on the computer to the 3G3MV.
Use the recommended commercially available USB-serial conversion cable.
4.The following restrictions apply when CX-One is used with Microsoft Windows Vista.
1) Some Help files cannot be accessed.
The Help files can be accessed if the Help program distributed by Microsoft for Windows Vista (WinHlp32.exe) is installed. Refer to the Microsoft homepage listed below or contact Microsoft for details on installing the file.
(The download page is automatically displayed if the Help files are opened while the user is connected to the Internet.)
http://support.microsoft.com/kb/917607/en-us
2) Restrictions apply to operation of some applications. Refer to the Setup Manual for details.
Support Software in CX-One Version 3.2
The following tables lists the Support Software that can be installed from CX-One
| Support Software in CX-One | Outline | |
| CX-Programmer | Ver.8.2 | Application software to create and debug programs for SYSMAC CS/CJ/CP/NSJseries, C-series, and CVM1/C-series CPU Units. Data can be created and monitored for high-speed-type Position Control Units. |
| CX-Integrator | Ver.2.3 | Application software to build and set up FA networks, such as Controller Link, DeviceNet, CompoNet, CompoWay, and Ethernet networks. The Routing Table Component and Data Link Component can be started from here. DeviceNet Configuration functionality is also included. |
| Switch Box Utility | Ver.1.6 | Utility software that helps you to debug PLCs. It helps you to monitor the I/O status and to monitor/change present values within the PLC you specify. |
| CX-Protocol | Ver.1.8 | Application software to create protocols (communications sequences) between SYSMAC CS/ CJ/CP/NSJ-series or C200HX/HG/HE Serial Communications Boards/Units and general- purpose external devices. |
| CX-Simulator | Ver.1.9 | Application software to simulate SYSMAC CS/CJ/CP/NSJ-series CPU Unit operation on the computer to debug PLC programs without a CPU Unit. |
| CX-Position | Ver.2.5 | Application software to create and monitor data for SYSMAC CS/CJ-series Position Control Units. |
| CX-Motion-NCF | Ver.1.8 | Application software to monitor and set parameters for SYSMAC CS/CJ-series Position Control Units and Servo Drivers that support MECHATROLINK-II communications. |
| CX-Motion-MCH | Ver.2.2 | Application software to create data for SYSMAC CS/CJ-series MCH Units, create motion programs, and perform monitoring. |
| CX-Motion | Ver.2.3 | Application software to create data for SYSMAC CS/CJ-series, C200HX/HG/HE, and CVM1/ CV-series Motion Control Units, and to create and monitor motion control programs. |
| CX-Drive | Ver.1.8 | Application software to set and control data for Inverters and Servos. |
| CX-Process Tool | Ver.5.2 | Application software to create and debug function block programs for SYSMAC CS/CJ-series Loop Controllers (Loop Control Units/Boards, Process Control CPU Units, and Loop Control CPU Units). |
| Faceplate Auto- Builder for NS | Ver.3.1 | Application software that automatically outputs screen data as project files for Ns-series PTs from tag information in function block programs created with the CX-Process Tool. |
| CX-Designer | Ver.3.1 | Application software to create screen data for NS-series PTs. |
| NV-Designer | Ver.1.0 | Application software to create screen data for NV-series small PTs. |
| CX-Configurator FDT | Ver.1.1 | Application software for setting various units by installing its DTM module. |
| CX-Thermo | Ver.4.1 | Application software to set and control parameters in components such as Temperature Control Units. |
| CX-FLnet | Ver.1.0 | Application software for system setting and monitoring of SYSMAC CS/CJ-series Fl-net Units. |
| Network Configrator | Ver.3.0 | Application software to set up tag data links for CJ2 (Built-in EtherNet/IP) CPU Units and EtherNet/IP Units. |
| CX-Server | Ver.4.3 | Middleware necessary for CX-One applications to communicate with OMRON components, such as PLCs, Display Devices, and Temperature Control Units. |
| PLC Tools (Installed automatically.) | A group of components used with CX-One applications, such as the CX-Programmer and CX- Integrator. Includes the following: I/O tables, PLC memory, PLC Setup, Data Tracing/Time Chart Monitoring, PLC Error Logs, File Memory, PLC clock, Routing Tables, and Data Link Tables. | |
Caution: In the interenst of product improvement, specifications are subject to change without notice.