![]()
Global
These are navigation links to move inside this page.
FA Integrated Tool Package
The CX-One is a comprehensive software package that integrates PLC Programming Software with Support Software for setting up Networks, Programmable Terminals, Servo Systems, Inverters, and Temperature Controllers.
![]()
Quick links to 'CXONE-AL[][]C-V3 / -AL[][]D-V3' page in your country / territory.
Please contact our European headquarters.
Get more support via Products links, such as manuals and CAD files.
FA Integrated Tool Package CX-One Version 3.[]: Better Than Ever
The PLC Programming Software Now Handles Position Control
The CX-One is a comprehensive software package that integrates PLC Programming Software with Support Software for setting up Networks, Programmable Terminals, Servo Systems, Inverters, and Temperature Controllers.
(New Feature 1)
The PLC Programming Software Covers Everything from Sequence Control to Position Control
The integration of Position Control Software into the PLC Programming Software greatly reduces the work required to set parameters, write programs, transfer data, and debug operation for Position Control Units. The parameter data is stored with the data for the PLC Programming Software to enable managing them together.
(New Feature 2)
Easily Set Up Synchronous Operation between Units
Setting up synchronous operation between SYSMAC CJ2 CPU Units and high-speed type Position Control Units is easily achieved on a visual interface.
(New Feature 3)
Support for SYSMAC CJ2 CPU Units without EtherNet/IP
(Upgrade)
Integrated Support Software Package for Compact PLCs
CX-One Lite
We've upgraded the CX-One Lite Software Package which is designed specifically for low end systems.
CX-One Networks
Windows is a registered trademark of the Microsoft Corporation. DeviceNet, DeviceNet Safety, CompoNet, and EtherNet/IP are trademarks or registered trademarks of the ODVA (Open DeviceNet Vendor Association). MECHATROLINK is a registered trademark of the MECHATROLINK Members Association. Other names of systems or products that appear in this document are trademarks or registered trademarks of the respective company.
(NEW)
Position Control Software Integrated into the CX-Programmer
Easily Achieve Position Control with Wading Through User Manuals
(Applicable Units: CJ1W-NC214/234/414/434)
Set Parameters for Position Control Units Together with Other PLC Settings Using the PLC Programming Software
Parameters for the high-speed-type Position Control Units can be easily set from the CX-Programmer. The parameters are saved in the CX-Programmer project file so you can manage them and transfer them together with the programs and other data.
Use Automatic I/O Comment Generation to Reduce Programming Work
I/O comments for parameters for high-speed-type Position Control Units can be easily generate, eliminating the need to refer to the user manual for the memory map of the Position Control Unit. This enables programming with I/O comments.
Easily Reuse Parameters for High-speed-type Position Control Units
You can compare and reuse the parameter data set for each axis.
(NEW)
Versatile Parameter Setting and Monitoring for Position Control
Complete Support for Synchronous Operation between Units
(Applicable Models: CJ2)
(Applicable Units: CJ1W-NC214/234/414/434)
Easy Setup of Synchronous Units
Just register to Synchronous Units to complete basic settings for memory allocations. If required, you can also easily customize the allocation parameters for the Synchronous Data Area.
Visually Monitor Status of Synchronous Operation between Units
You can display status lists for Synchronous Operation between Units operation to easily check Units with error.
Easily Import CAM Data
You can easily import data created with the CAM editor into the PLC memory component.
Note:The WS02-MOPC2 CAM Data Creation Software (sold separately) is required to create CAM data.
(NEW)
USB and EtherNet/IP Ports are Standard Features for SYSMAC CJ2 CPU Units
Easier and Safer Connection to PLCs
(CX-Programmer)
(Applicable Models: CJ2)
Easy connection with USB
A standard USB cable can be easily connected to the USB port on the front of the CPU Unit.
Easy Connection with EtherNet/IP
Easy connection by specifying the computer LAN (Ethernet) port and IP address only.
Prevent Connection Errors by Verifying PLC Names
The CJ2 CPU Unit can record a PLC name. Errors in transfers can be prevented ahead of time because the PLC name can be compared with what is in the project file when connecting online.
Browse and Connect from the EtherNet/IP Connection List
Even if the IP address is unknown, you can browse a list of PLCs connected to the EtherNet/IP and select one to connect to it. With this, remote debugging and maintenance can be conducted smoothly on site.
(NEW)
Integration of Network Construction and Parameter Settings
Now Supports EtherNet/IP and CompoNet
EtherNet/IP and CompoNet are now supported in addition to previously supported Ethernet, Controller Link, and DeviceNet networks.
High-speed and high-capacity data links are possible with EtherNet/IP, and synchronization cab be specified for each application without depending on the number of nodes.
EtherNet/IP Datalink Tool
The addresses can be set for EtherNet/IP data links using data link tables.
(Network Configurator)
EtherNet/IP Support
(Network Configurator)
CompoNet Support
(CX-Integrator)
(NEW)
Data can be easily managed for the entire PLC system and down time in an emergency can be minimized
Batch Backup/Restore with a Computer
A computer can be used to backup, compare, or restore data for all or specific PLC Units when connected online. Backup information is automatically tagged with a date stamp. It is thus possible to return to the state before an error occurred. It is also easy to identify the file for restoring data when an error occurs.
Applications
Backup of all data transferred to the PLC
Batch transfer of all data to a PLC with the same configuration (using the restore function)
Transfer of relevant data to a new Unit installed after a Unit has failed
Backup Data
CPU Unit programs, data memory, and PLC Setup
Settings for CPU Bus Units and Special I/O Units in the PLC
Comprehensive Programming Environment with Single-key Operation and Flexible Multilingual Support
In addition to practical functions such as single-key operation that improves the programming efficiency, processing is conducted in the optimal language. Flexible multilingual support and the Smart Libraries enable a comprehensive programming environment.
Improved Programming Efficiency with Single-key Operation
The CX-Programmer features the "Single-key Concept" to increase operability. Apart from inputs to ladder diagrams, history searches, and model jumps, single-key operation can be used for simulation debugging as well.
Excellent Operability Makes Programming and Debugging Easy
Multiple Languages Can Be Combined To Make Programming Flexible
The multilingual feature supports IEC 61131-3. Programming is possible in a language that is appropriate for the process by combining ladder diagram and ST languages. Function blocks can be created to make programming even more efficient.
Smart Libraries (Smart FB Library, SAP)
Ladder diagrams, communications programs, and control screens can be created simply by selecting and pasting program modules from the extensive libraries.
Using FB and SAP modules to build the programs, it is possible to create programs that are easier to understand.
(NEW)
Diversity of Programs Is Top Class in the Industry
High Program Readability
OMRON has refined the programming environment so that programs can be designed and written efficiently with minimal errors, high readability, and adaptability to changes in specifications.
Programming with Symbols
Data Specification Is Easy To Understand with Array Variables (Array Symbols)
Programs are easy to understand because data string sequences can be described with subscripts. This feature can also be used for network symbols. Therefore exchanges of multiple data with external devices can be easily written.
(Available languages: Ladder diagrams, ST, and SFC)
Example: Array variable: ABC
Symbols Can Be Used As Subscripts for Array Variables
Data can be dynamically specified by using physical addresses and symbols as the subscripts to arrays.
(Applicable Models: CJ2)
Example:
data[i]: Indirect specification of an element number using symbol i
If symbol i is &5, it specifies the 5th element in the array
Usability Has Improved Also for Programming Using Addresses
DM/EM Bits Can Be Addressed
Bits could not be addresses in the DM and EM Areas with the previous SYSMAC CPU Units, but now it is possible with the CJ2. Programs with high readability can now be created.
(Applicable Models: CJ2)
Example: D100.05: D100 bit 05, E0_100.03: E0_100 bit 03
Address Offsets Can Be Specified
Offsets from a specific starting bit address or word address can be specified in programming. Addresses can be dynamically specified with the contents of a word by specifying the specific address in I/O memory as the offset. This way it is possible to create programs in a similar way to using index registers.
(Applicable Models: CJ2)
Example 1:
D100[5]: Take D100 as the first address and add an offset of 5 words to specify D105
Example 2:
10.00[5]: 10.00[5]: Take CIO 10.00 as the starting bit address and add an offset of 5 bits to specify CIO 10.05
Example 3:
D100[W100]: Take D100 as the starting address and add the contents of W100 as the offset
If the contents of W100 is &5, D105 is specified
Comprehensive Help for New CJ2 Instructions
Support is provided for tracking and sorting instructions, communications instructions, and instructions for finding maximum or minimum floating-point values.
Comprehensive Debugging for Networks
Time Required for Onsite Startup and Debugging Has Been Significantly Reduced
With CX-One version 3.0, debugging is efficient with simultaneously monitoring and management of multiple networks and PLCs.
Management of Multiple Networks
The operation of networks with configurations consisting of multiple networks including PLC networks such as EtherNet/IP and Controller Link, field networks such as DeviceNet and CompoNet, and networks for Programmable Terminals and Serial Devices, can be restored simultaneously from the CX-One. Onsite start up and debugging can be conducted efficiently and without errors because PLCs and devices can be selected from the window to transfer programs and parameter data to the computer during operation.
Ladder diagram Monitoring for Multiple PLCs
Multiple PLCs can be monitored by displaying them in series on the screen. This way it is easy to debug data links between PLCs and monitor the inputs and outputs of different PLCs.
Group Monitoring of Multiple PLC Input/Outputs in the Watch Window
The desired I/O data can be selected for multiple PLCs, such as input bits, output bits, and word I/O data, and monitored simultaneously. There are also functions such as the Binary Monitor and Forced Set/Reset functions that enables graphical monitoring the ON/OFF status of word data. All of these monitoring functions are easy to use.
(Ver.up)
Time Require for Debugging and Maintenance Has Been Reduced with the Comprehensive Data Trace Function
Functionality and operability has been significantly upgraded compared to the previous data trace function. The new data trace function provides comprehensive debugging, such as I/O comment display of sampled addresses, specification using symbols, checking the measurement time between two selected points, and layering waveforms. Furthermore, data sampled from the CPU Unit's trace memory can be saved to a file on the computer at a specified frequency. This can be used as for long-term logging of data.
Data Trace Function
Continuous Data Trace Logging
(Applicable Models: CJ2)
Simulation Debugging
Programs can be debugged using a computer without the actual PLC. A wide range of languages, such as ladder diagram, sequential function charts (SFC), structured text (ST), and programs within function blocks are supported. Furthermore, programs can be edited online, bits can be forceset/reset, breakpoints can be set, and a PLC error simulator can be used.
Simulation of SFC, Ladder Diagrams, and Function Blocks
No Size Restrictions for Online Editing of Function Blocks and Sequential Function Charts
There are no size restrictions for the function blocks and SFC that can be edited online.
(Applicable Models: CJ2)
Products Are Highly Compatible and Easy to Use Because They Are from a Comprehensive PLC Manufacturer
The CX-Designer Simplifies the Processes from Screen Design to Debugging for the NS-series Programmable Terminals
The time required for designing can be significantly reduced because of the compatibility with SYSMAC CJ-series PLCs. The process of designing screens is easier with expanded functionality.
(Applicable Units: NS Series, NSJ Series)
Communications Components and the Smart Active Parts (SAP) Library Significantly Reduces the Time Required to Create Ladder Diagrams and Screens
There are over 3,000 Smart Active Parts that can directly access OMRON PLCs and components. Simply select and paste a part from the SAP library onto the screen. Detailed screens and ladder diagrams do not need to be created.
Using Software Components, Error Checking and Parameter Setting Can Be Done without a Computer
There are many software components in the Software Function SAP Library that can be easily incorporated into the NS-series Programmable Terminals.
Simply select and paste software components on the screen. Device errors can be checked and parameters set without a computer.
The Troubleshooter SAPs Can Be Used Onsite without Computers or Manuals
There is a troubleshooter SAP library that covers all PLC Units. If there is a PLC error, the troubleshooter SAP library explains the cause and how to implement countermeasures in a way that it is easy to understand.
Improved Troubleshooter SAP Library
In addition to the DeviceNet Units and Position Control Units, the CX-Designer also includes Basic I/O Unit, Analog I/O Units, Serial Communications Units, High-speed Counter Units, Controller Link Unit, and ID Sensor Units. Including the EtherNet Units and Motion Control Units is planned in future development stages.
Integrated Simulation with the PLC Ladder Diagrams
Test functions for the CX-Designer and CX-Programmer are linked through the CX-Simulator on a computer. This enables screens and ladder diagrams to be checked simultaneously, significantly improving the debugging efficiency. A new Integrated Simulation Button has been added to the CX-Programmer.
Furthermore, work efficiency has been significantly improved with the function that enables work windows to be pinned in front, and a flexible zoom function.
Screens and Ladder Diagrams Can Be Simultaneously Checked on a Computer
The Comprehensive Screen Designing Software Makes for Easy Creation of Multifunction Screens
A Multifunction Object is a collection of the functions of various objects. Multiple functions can be operated with a single press of a button without using cumbersome macros. Setting Multifunction Objects is easy. For example, you can visually create a setting like "Change the screen when the device operation start bit turns ON and the value is set" using the software.
Operation of multiple functions can be achieved with a single hit of a button without using macros
Easy and visual software settings
Use the NV-Designer to Easily and Quickly Design Screens for the NV Series of Compact PTs
(Applicable Units: NV Series)
Easy High-level Servomotor Control
The CX-Motion Supports Motion Network Servo Systems
Improve productivity of motion network servo systems using MECHATROLINK-II for design, startup, and maintenance.
Easy Management of Parameters While Still Connected to PLCs CX-Motion-NCF
Even Easier to Start Up a System CX-Motion-MCH
From Parameter Settings to Temperature Data Management
The CX-Thermo/CX-Process Software Supports High-level Temperature Control
Setting Temperature Controller Parameters Is Easier CX-Thermo
Parameters can be easily set from a list
Easy Parameter Settings
Parameters can be set even for Temperature Controllers that do not support communications.
Parameters can be saved, and then copied, or reused and edited (Parameters can be exported in CSV or HTML format.)
Displays Only What Is Used
To avoid unintentional use of parameters, unused parameters can be masked (i.e., hidden)
Applicable Units:
E5CN/E5CN-H/E5AN/E5AN-H/E5EN/E5EN-H, EJ1, E5ZN, E5AR/E5AR-T/E5ER/E5ER-T
*The DeviceNet type is excluded
Programming for the Process Controller Is Easier CX-Process
Control Programs Can Be Constructed By Pasting Function Blocks
Control Can Be Customized
Control programs can be constructed by pasting function blocks and connecting them. They can be used for simple PID control, program control, and cascade control.
Easy Creation of an HMI
Screens for the NS-series PTs (NS runtime screen) are automatically generated from the function block programs. Standard control screens and tuning screens do not need to be created manually.
Applicable Units:
CJ1G-CPU4[]P/CPU4[]P-GTC, CS1W-LCB01/LCB05/LCB05-GTC, CS1W-LC001, CS1D-CPU6[]P
CX-Thermo/CX-Process Support Software
Adjusting Parameters While Monitoring Trends
PID parameters can be adjusted while monitoring the present value (PV), setting point (SP), and manipulated variable (MV). Trend data can be saved in CSV format.
(CX-Thermo Trend Viewer, CX-Process Support Software Tuning Screen)
Controlling with a Reliable Control Algorithm (See note.)
The execution of the autotuning (AT) function that calculates the PID constants and the fine tuning (FT) function that improves controllability exactly as required are made easy with an intuitive user interface. The interference overshooting adjustment function is supported to adjust overshooting when interference occurs, and the gradient temperature control function achieves constant internal temperatures for multi-point temperature control with interference.
Note:Supported functions depends on the product being used. Refer to product manuals for details.
(NEW)
Easily write programs to read and write PLC data with VB or VC#.
CX-Compolet
Easy to Use without Any Technical Knowledge
Provides software components that help you easily and quickly develop PLC communications.
Read and write PLC data without the need to consider differences between networks.
Supports Microsoft Visual Studio .NET 2008.
For the CJ2 with EtherNet/IP functionality, I/O memory in the PLC can be accessed by using tag names rather than addresses.
Array variable access is possible.
(NEW)
Communications Middleware to Connect a Computer and SYSMAC PLCs
SYSMAC Gateway
Direct Connection of the Industrial Ethernet: EtherNet/IP
Direct Access to High-speed and High-capacity Networks
In addition to FINS communications, operation of SYSMAC Gateway has been verified on EtherNet/IP.
Absorbs differences in the physical layer between RS-232C, USB, Ethernet, EtherNet/IP, and Controller Link.
Just install the software on the computer to enable data communications for controls and information.
Note:Communications are possible via USB and Ethernet too.
Web Support Services for CX-One
OMRON'S CX-One offers many service options in the Internet environment so that engineers and online support is available from anywhere in the world 24 hours a day.
Online User Registration
When you register online as a user of CX-One, all CX-One software components can be registered at once. The online registration website can be accessed from Japan, North America, South America, Central America, Europe, Africa, Asia, China, Taiwan, and Korea. You can access the Internet services from anywhere once you have registered.
Automatic Update
With the automatic update function of CX-One, the latest update information for your computer environment can be searched for and applied using the network environment. Your CX-One can be constantly updated to the latest state. It is also possible to update only the necessary tools.
Download Services
Control devices that were made available after you purchased the Support Software can be used if you download the latest Smart Libraries from the Internet. A customized library can be made by downloading the Smart FB Library and Smart Active Parts for the hardware that you require. Programming is also easy by selecting and pasting the necessary parts.