![]()
Global
These are navigation links to move inside this page.
Analog I/O Terminals
Performs Calculations on Analog Values within the Slave Itself. Also Provides High Resolution at 1/30,000 (Full Scale) and Support for a Wide Variety of Data Sampling.
![]()
Quick links to 'DRT2-AD04(H) / DA02' page in your country / territory.
Please contact our European headquarters.
Get more support via Products links, such as manuals and CAD files.
Equipped with the standard Smart Slave functions that provide powerful preventative maintenance and troubleshooting capabilities.
Sampling data can be analyzed internally to provide a low-cost scheduler function.
Equipped with functions such as the scaling function, peak/bottom hold; top/valley hold; comparator function, cumulative counter, and derivative calculation function.
Two I/O points can be allocated to any two of the following values: analog input, peak/bottom, top, valley, or rate-of-change. Values without an allocated I/O point can be read with message communications.