Page top

Lead Contents

Pushbutton Switch (Detachable) (Lighted/Non-Lighted) (Cylindrical 16-dia.)

A16

A16

Separate Construction with Cylindrical 16-dia. Body

Primary Contents



The Dimension shows 2-switch outputs.

The lamp terminal is also provided with non-lighted models.

Rectangular
A16[]-J
Solder terminals (tab terminals #110)

A16[]-J_Dim

Square
A16[]-A
Solder terminals (tab terminals #110)

A16[]-A_Dim

Round
A16[]-T
Solder terminals (tab terminals #110)

A16[]-T_Dim

The Dimension shows 2-switch outputs.

The lamp terminal is also provided with non-lighted models.

A rectangular model is listed as an example.

Rectangular
A16[]-J[]-[]P
PCB terminals

A16[]-J[]-[]P_Dim

Rectangular
A16[]-J[]-T1
Voltage-reduction lighting, solder terminals (tab terminals #110)

A16[]-J[]-T1_Dim

Rectangular
A16[]-J[]-2S, T1-2S, T2-2S
Screw-less Clamp

A16[]-J[]-2S_Dim

Lamps

LED
A16-5D[]/-12D[]/-24D[]

A16-5D[]_Dim

*The voltage display surface is the same color as the illumination color. The opposite surface is light gray.
(For pure white, the entire surface is light gray.)

Incandescent Lamp
A16-5/-12/-24

A16-5_Dim

Accessories, Tools, and Components

Extractor
A3PJ-5080

A3PJ-5080_Dim

Legend Plates

A16ZJ-520[]

A16ZJ-520[]_Dim

A16ZT-520[]

A16ZT-520[]_Dim

A16ZA-520[]

A16ZA-520[]_Dim

Note:
1. The panel is 0.6 mm thick.
2. The panel is made of the materials listed in the following table.

A16_Legend Plates

Screw Fitting
A16Z-3004

A16Z-3004_Dim

Panel Plugs (Black Resin)

Select the Plug that fits the panel design and mount from the front of the Panel. Panel cutouts are the same as those for Switches.
Protective structure: IP40
Color: Black

A16_Panel Plugs

Lock Ring

A16_Lock Ring_Dim

Socket Unit Lamp Extractor
A16Z-5080

A16Z-5080_Dim

Panel Cutouts

Solder Terminals and Screw-less Clamp Connectors

A16_Panel Cutouts1

Note:
Make sure the thickness of the mounting panel is between 0.5 and 3.2 mm. If, however, a Switch Guard or Dust Cover is used, the thickness of the mounting panel must be between 0.5 and 2 mm.
If the panel is to be finished with coating, etc., make sure that the panel meets the specified dimensions after coating.
Figures in parentheses are for Screw-less Clamp Connectors.

PCB Terminals

A16_Panel Cutouts2

Note:
Ensure that the variation in the distance between the centers of neighboring mounting holes is less than ±0.1 mm.
Make sure the thickness of the mounting panel is between 0.5 and 3.2 mm. If, however, a Switch Guard or Dust Cover is used, the thickness of the mounting panel must be between 0.5 and 2 mm.
If the panel is to be finished with coating, etc., make sure that the panel meets the specified dimensions after coating.

Accessory Dimensions Mounted

Dimensions with Switch Guard Installed

Rectangular
A16ZJ-5050

A16ZJ-5050_Dim

Note: This example is for when X is 4.5 mm.
If X is not required, the Switches can be mounted with a minimum vertical installation pitch of 24 mm min.

Square
A16ZA-5050

A16ZA-5050_Dim

Note: This example is for when X is 4.5 mm.
If X is not required, the Switches can be mounted with a minimum vertical installation pitch of 24 mm min.
If PCB terminals are used, provide X must be 24 mm or larger.

Dust Covers

Rectangular
A16ZJ-5060

A16ZJ-5060_Dim

Square
A16ZA-5060

A16ZA-5060_Dim

Round
A16ZT-5060

A16ZT-5060_Dim

Caution: All units are in millimeters unless otherwise indicated.