![]()
Global
These are navigation links to move inside this page.
ID Tags manage data on warehouse receiving and shipping for engines to transport between factories.
An RFID system obtains traceability data to manage warehouse receiving and shipping of engines.
Introduction of an RFID system enables transfer and linking of data between the engine factory and vehicle factory.
The management of data at the host automates data collection and management of engine receiving and shipping at the warehouse.
An ID Tag is installed on the tray that holds engines. Data reading/writing is performed between the Antenna on the stoker and the ID Tag on the tray. This is done for management when a forklift transfers a tray to or from the stocker.
The use of RFID which automatically reads and writes data can reduce more processing time than the use of barcodes which are read manually. Data communications between factories makes it easy to link engine data.
Application No.326
New, Next-generation RFID Systems with ISO/IEC 18000-3 (ISO/IEC15693) Compliance
![]()
Quick links to 'V680 series' page in your country / territory.
Please contact our European headquarters.
Get more support via Products links, such as manuals and CAD files.