Page top

Primary Contents



When the cassette rack is mounted to the mounter, the information for all of the cassettes and placement information are read by the Antenna installed on the mounter, and a comparison is made to determine whether the correct cassettes have been loaded (that is, whether the mounting program is correct).

Know-How

The information that was previously managed by bar codes (parts number, parts name, quantity, etc.) can be automatically compared for the cassettes by using the ID Tag. Also, whereas bar codes were subject to soiling, ID Tags are highly resistant to soiling.

Benefit / Efficiency

The parts that are supposed to be loaded into the cassette rack and the parts that are required by the mounting program are reliably compared, thus preventing errors and dramatically reducing costs due to loss. Even if the combination of cassettes loaded into the cassette rack changes, the information in the ID Tag can simply be rewritten, allowing simple and detailed cassette control.

RFID System
RFID System V680 series

New, Next-generation RFID Systems with ISO/IEC 18000-3 (ISO/IEC15693) Compliance